USB DFU UUID or OTP Access

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB DFU UUID or OTP Access

1,299 Views
travis_scott
Contributor II

We are using LPC54616 MCUs in a product. We want to enable field upgrades of these devices using USB DFU. Is it possible to read the OTP (which is set with serial number during production) or the MCU UUID through the USB DFU bootloader in ROM? That way we can uniquely identify the product.

Thanks

0 Kudos
Reply
1 Reply

1,224 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Travis,

 

The only options you have to read the UID is the IAP ReadUID command or the USART ReadUID command through ISP.

 

I recommend you to check chapter 5.6.9 and 5.4.5.15 respectively in the User Manual.

 

I hope this helps you.

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply