CANFD receive error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CANFD receive error

1,694 Views
黎明孟
Contributor II

LPC54618 CANFD receive error:

The OM13094UL board used for CANFD and 500k/5M Baudrate used for communication;

It seems OK when only transmit out the data, the VehSpy used to monitor the CANFD frame;

 

But when use VehSpy to send the data to the board, the bus error occured;

As follow:

 

 

 

 

 

 

and when the bit rate switch disable, seems normal with VehSpy sending;

Labels (1)
0 Kudos
Reply
1 Reply

1,589 Views
FelipeGarcia
NXP Employee
NXP Employee

This is a duplicated thread of: https://community.nxp.com/thread/503213 

0 Kudos
Reply