USB DFU UUID or OTP Access

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB DFU UUID or OTP Access

1,314 次查看
travis_scott
Contributor II

We are using LPC54616 MCUs in a product. We want to enable field upgrades of these devices using USB DFU. Is it possible to read the OTP (which is set with serial number during production) or the MCU UUID through the USB DFU bootloader in ROM? That way we can uniquely identify the product.

Thanks

0 项奖励
回复
1 回复

1,239 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Travis,

 

The only options you have to read the UID is the IAP ReadUID command or the USART ReadUID command through ISP.

 

I recommend you to check chapter 5.6.9 and 5.4.5.15 respectively in the User Manual.

 

I hope this helps you.

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复