USB Composite Audio + HID DEMO LPC55S28

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Composite Audio + HID DEMO LPC55S28

ソリューションへジャンプ
4,163件の閲覧回数
Claudio_ML
Contributor II

I'm testing example project COMPOSITE HID AUDIO Unified bare metal from SDK 2.11 on a LPCXpresso55s28.

Audio Speaker profile is working fine but Line IN/Microphone profile is not sending data from board to PC

I also noted that Microphone volume under Windows properties is fixed to 0 (zero)

Any idea on what I'm getting wrong?

Thank you

0 件の賞賛
返信
1 解決策
4,127件の閲覧回数
Claudio_ML
Contributor II

Thank You Alice, I already did the check you mentioned.

Anyway I found the problem, #define USB_DEVICE_CONFIG_AUDIO_CLASS_2_0 is not seen on all project files and this makes some part not working accordly with AUDIO Class 2.0, making it visible by all fix the issue.

Claudio

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,128件の閲覧回数
Claudio_ML
Contributor II

Thank You Alice, I already did the check you mentioned.

Anyway I found the problem, #define USB_DEVICE_CONFIG_AUDIO_CLASS_2_0 is not seen on all project files and this makes some part not working accordly with AUDIO Class 2.0, making it visible by all fix the issue.

Claudio

0 件の賞賛
返信
4,137件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Claudio_ML,

Have you refer to the steps of readme.pdf, pay particular attention to the note at the end of the document.

I attach it for you.

 

BR

Alice

0 件の賞賛
返信