USB Composite Audio + HID DEMO LPC55S28

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB Composite Audio + HID DEMO LPC55S28

跳至解决方案
4,158 次查看
Claudio_ML
Contributor II

I'm testing example project COMPOSITE HID AUDIO Unified bare metal from SDK 2.11 on a LPCXpresso55s28.

Audio Speaker profile is working fine but Line IN/Microphone profile is not sending data from board to PC

I also noted that Microphone volume under Windows properties is fixed to 0 (zero)

Any idea on what I'm getting wrong?

Thank you

0 项奖励
回复
1 解答
4,122 次查看
Claudio_ML
Contributor II

Thank You Alice, I already did the check you mentioned.

Anyway I found the problem, #define USB_DEVICE_CONFIG_AUDIO_CLASS_2_0 is not seen on all project files and this makes some part not working accordly with AUDIO Class 2.0, making it visible by all fix the issue.

Claudio

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,123 次查看
Claudio_ML
Contributor II

Thank You Alice, I already did the check you mentioned.

Anyway I found the problem, #define USB_DEVICE_CONFIG_AUDIO_CLASS_2_0 is not seen on all project files and this makes some part not working accordly with AUDIO Class 2.0, making it visible by all fix the issue.

Claudio

0 项奖励
回复
4,132 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Claudio_ML,

Have you refer to the steps of readme.pdf, pay particular attention to the note at the end of the document.

I attach it for you.

 

BR

Alice

0 项奖励
回复