USB Composite Audio + HID DEMO LPC55S28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Composite Audio + HID DEMO LPC55S28

Jump to solution
4,136 Views
Claudio_ML
Contributor II

I'm testing example project COMPOSITE HID AUDIO Unified bare metal from SDK 2.11 on a LPCXpresso55s28.

Audio Speaker profile is working fine but Line IN/Microphone profile is not sending data from board to PC

I also noted that Microphone volume under Windows properties is fixed to 0 (zero)

Any idea on what I'm getting wrong?

Thank you

0 Kudos
Reply
1 Solution
4,100 Views
Claudio_ML
Contributor II

Thank You Alice, I already did the check you mentioned.

Anyway I found the problem, #define USB_DEVICE_CONFIG_AUDIO_CLASS_2_0 is not seen on all project files and this makes some part not working accordly with AUDIO Class 2.0, making it visible by all fix the issue.

Claudio

View solution in original post

0 Kudos
Reply
2 Replies
4,101 Views
Claudio_ML
Contributor II

Thank You Alice, I already did the check you mentioned.

Anyway I found the problem, #define USB_DEVICE_CONFIG_AUDIO_CLASS_2_0 is not seen on all project files and this makes some part not working accordly with AUDIO Class 2.0, making it visible by all fix the issue.

Claudio

0 Kudos
Reply
4,110 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Claudio_ML,

Have you refer to the steps of readme.pdf, pay particular attention to the note at the end of the document.

I attach it for you.

 

BR

Alice

0 Kudos
Reply