Hello everyone,
I have configured the UART1 of my LPC2148 with speed: (9600 / 8bits / N /1bit Stop) with interruption. The UART1 connects to an ESP-01 I can send and receive information perfectly. The problem I present is when receiving a certain amount of data from the ESP-01, the microcontroller for some reason stops transmitting information and I do not understand what the reason is. below I leave the configuration and the information that I am receiving from the ESP, when receiving 6 times this frame the microcontroller stops.
Data frame:
//----------------------------------------Data frame received---------------------
+IPD,4,346:HTTP/1.1 200 OK
Server: xxxxx/x.x.xx (xxxxxx)
Vary: Accept-Encoding
Content-Length: 155
Connection: close
Content-Type: text/html; charset=UTF-8
[{"count":"6","image":"0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF,
0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF,"}]
OK
//------------------------------------------------------------------------------
Code:
//----------------------------Structure for Data recieved------------------------------------------
typedef struct {
int in;
int out;
char buffer[400];
}p;
p *ptr2,datos_serial2;
//---------------------------Init UART1---------------------------------------------
void uart1_init(void)//9600 BAUD pclock 48MHZ
{
PCONP |= 0x00000010;/* PCRTC = 1 */
PINSEL0 |= 0x00050000; /* Enable RxD1 and TxD1*/
U1LCR=0X83; //8-data bits, 1 Stop bit, Disable Parity and Enable DLAB
U1DLL=0x38;// MULVAL = 0x5 and DIVADDVAL = 14
U1DLM=1;
U1LCR=0X03; //cleared DLAB
U1IER= 0x00000001;//Enable Interrupt
}
//---------------------------------Send Char----------------
void SendCharUART1 (char str){
U1THR = str;
while( (U1LSR & 0x40) == 0 ); /* Wait till THRE bit becomes 1 which tells that transmission is completed */
}
//--------------------------------Interrupt enable------------------------------------------------------
void UART1_Interrupt_EN(void)
{
// VICIntSelect = 0x00000000;
VICVectAddr7 = (unsigned) UART1Handler;//Vector 7
VICVectCntl7 = 0x00000020 | 7; //select UART1 interrupt as IRQ i.e vector 7
VICIntEnable |=(1UL<<7);//interrupt ena.
}
//------------------------------------------Interrupt IRQ--------------------------------------------
void UART1Handler (void) __irq
{
// /* Serial Receive Interrupt. */
char recieved;
if ((U1IIR & 0x0E) == 0x04) {
recieved=U1RBR;
ptr2 = &datos_serial2;
if(ptr2->in>=399)
ptr2->in=0;
ptr2->buffer[ptr2->in++]=recieved;
}
VICVectAddr = 0x00;
}
//-----------------------------------------Main-------------------
int main()
{
uart1_init();
UART1_Interrupt_EN();
while(1){
sendata_esp01(); //Process to send data to ESP01
delay()
//----------------- Algorithm to process the received data------------------//
Process_Datareceived();
//--------------------------------------------------------------------------------------//
}
}