UART connection for LPC55S28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART connection for LPC55S28

1,061 Views
steve5528
Contributor I

Good day!

 

I am building a PCB with LPC55S2x and would like to know the hardware level specifics to make UART work? If for instance, FC0 UART is being used, then, is it simple as routing the two FC0 pins: RXD and TXD to a jumper from where a serial-usb bridge is used to connect to the PC? Do RX and TX lines need any resistors on their path? In EVK-LPC55S2x schematics, I see FC0_USART_RXD connecting to a 100 ohm resistor, so wanted some clarification.

 

Thanks.

0 Kudos
Reply
1 Reply

1,031 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @steve5528 

We highly recommend that you refer to the schematic of the LPCxpresso55s28.

https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools...  

 

BR

Alice

0 Kudos
Reply