UART RECEIVE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART RECEIVE

12,864件の閲覧回数
DHARSAN
Contributor III

Hi,

    How to receive transmitted data in UART in interrupt method without using DMA in LPC55S16?

0 件の賞賛
返信
4 返答(返信)

12,818件の閲覧回数
DHARSAN
Contributor III

I have attached the images. 1st picture is MCU IDE which i had debugged for receive from the UART MAX232 in USR_TCP

 

0 件の賞賛
返信

12,831件の閲覧回数
DHARSAN
Contributor III

Hello Alice,

I had worked with the SDK example which you had mentioned above. The transmission succeed to the UART mode from the controller but couldn't get the receiving data from the module to the LPC55S16 microcontroller. Can you suggest some other way?

Best Regards

Dharsan K K

0 件の賞賛
返信

12,772件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DHARSAN 

Do you connect  serial terminal on PC with your LPC55s16 board? 

I tested with this demo, work well without any change.

Have you tested with default demo? 

 

BR

Alice

0 件の賞賛
返信

12,847件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DHARSAN 

How about refer to the demo "usart_9bit_interrut_transfer" under SDK?

Alice_Yang_0-1715844574195.png

 

BR

Alice

 

0 件の賞賛
返信