UART RECEIVE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UART RECEIVE

13,226 次查看
DHARSAN
Contributor III

Hi,

    How to receive transmitted data in UART in interrupt method without using DMA in LPC55S16?

0 项奖励
回复
4 回复数

13,180 次查看
DHARSAN
Contributor III

I have attached the images. 1st picture is MCU IDE which i had debugged for receive from the UART MAX232 in USR_TCP

 

0 项奖励
回复

13,193 次查看
DHARSAN
Contributor III

Hello Alice,

I had worked with the SDK example which you had mentioned above. The transmission succeed to the UART mode from the controller but couldn't get the receiving data from the module to the LPC55S16 microcontroller. Can you suggest some other way?

Best Regards

Dharsan K K

0 项奖励
回复

13,134 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DHARSAN 

Do you connect  serial terminal on PC with your LPC55s16 board? 

I tested with this demo, work well without any change.

Have you tested with default demo? 

 

BR

Alice

0 项奖励
回复

13,209 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @DHARSAN 

How about refer to the demo "usart_9bit_interrut_transfer" under SDK?

Alice_Yang_0-1715844574195.png

 

BR

Alice

 

0 项奖励
回复