UART Bootloader LPC55S16

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART Bootloader LPC55S16

1,834 Views
RRD101
Contributor III

Did I understand the table "Table 195. ISP pin assignments" correctly, that a bootloader which uses the UART interface is only usable with Flexcomm0 and i2c only with Flexcomm1? Or can I use UART also with Flexcomm1?

 

BR

Ralf

0 Kudos
Reply
2 Replies

1,819 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello @RRD101 ,

The ISP boot is available on the following serial interfaces:

- UART0

- I2C1

- SPI3

- USB0_FS

- USB1-HS

So answering your question yes the USART ISP mode is only available on the FC0. Please let me know if you find this information useful.

0 Kudos
Reply

1,775 Views
RRD101
Contributor III

Hi @nxf77486 ,

i think it wasnt the correct answer on what i initially ment. i think what i mean is a secondary bootloader. could it be, that i can use any FC i want for UART there?

 

BR

Ralf

0 Kudos
Reply