Hi,
I am testing the UAC on lpcxpresso55s28 using the sample code dev_audio_speaker_freertos from the SDK SDK_25_03_00_LPCXpresso55S28. The default 2 channel UAC is ok. But when I try to configure it to 5.1-channel following the document "Implementation of 5.1-channel Audio Solution on LPC55xx", it seems not working. Because I click the "configure" button for the UAC speaker, there is no window pops up like below. Please help to check it. Thanks!