Timer/RIT: write clear interrupt flag to 1, read as 0, when?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Timer/RIT: write clear interrupt flag to 1, read as 0, when?

1,281件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by petekol on Sun Nov 01 07:04:59 MST 2015
Hi

i have some understanding problem of clearing an interrupt flag of RIT:
i expect that harware clears the flag to 0 and a can read it as 0 after i write 1 to it. In practice i do not read 0 event if doing it in a loop for ever (in ISR).

Does it means that it is acctually cleared internally by writing 1 an i can't read it as 0 (only after exit from ISR?) but if i move compare value then it fire interrupt next time.

So tha question is when i should expect to read the flag as 0? Before this time and after i write 1 to it can i trigger one more compare fire (flag goes to 1)?

Thnx
Lok
ラベル(1)
0 件の賞賛
返信
0 返答(返信)