Boot code for new board having LPC4350

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot code for new board having LPC4350

968 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by prathiba on Wed Feb 27 04:18:06 MST 2013
Hi All ,
Previously we were using NXP Hitex board with LPC43xx.Now We are using  the custom  board , which is having the lpc4350 as the main processor.I want to know how start with this new board .We are using S25FL256S as an external flash. The problems I am facing are
1.ULink2 is not detecting with this board.
2.So the board has to be programmed with the boot code first or what is the other way to do ?
3.If boot code is required , where I will get the code for it ?

Please Help me .
Thanks in advance
SaiSmita
Labels (1)
0 Kudos
Reply
0 Replies