The question of LPC2929

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The question of LPC2929

859件の閲覧回数
1263906294
Contributor I

1、I would like to ask does this ARM9 LPC2929 chip have on the power sequence requirements?

2、If I want to use a LPC2929 plug-in FLASH, I would like to ask at least how much FLASH?

0 件の賞賛
返信
1 返信

747件の閲覧回数
b36401
NXP Employee
NXP Employee

1.

LPC2929 operates in normal-power mode after reset. In this mode the device is fully functional. The system can be put into idle-power mode either partially or fully.
LPC2929 contains external reset input and internal power-up reset circuits. This ensures that a reset is internally extended internally until the oscillators and flash have reached a stable state.

2.

LPC2929 has 768kB flash memory.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信