The question of LPC2929

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The question of LPC2929

1,200 次查看
1263906294
Contributor I

1、I would like to ask does this ARM9 LPC2929 chip have on the power sequence requirements?

2、If I want to use a LPC2929 plug-in FLASH, I would like to ask at least how much FLASH?

0 项奖励
回复
1 回复

1,088 次查看
b36401
NXP Employee
NXP Employee

1.

LPC2929 operates in normal-power mode after reset. In this mode the device is fully functional. The system can be put into idle-power mode either partially or fully.
LPC2929 contains external reset input and internal power-up reset circuits. This ensures that a reset is internally extended internally until the oscillators and flash have reached a stable state.

2.

LPC2929 has 768kB flash memory.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复