Test registers of SPI module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Test registers of SPI module

1,036件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Divya on Mon Oct 28 02:17:30 MST 2013
What for SPI Test Status Register and SPI Test Control Registers are used in SPI module?
Please explain with scenario.
Thanks in advance.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,025件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Wed Nov 06 16:47:26 MST 2013
from UM10503.pdf
Note that the bits in this register are intended for functional verification only. This register should not be used for normal operation.

most likely these are registers that are used for internal NXP testing
to test the peripheral.
they probably do not need to be mentioned in the manual, but some one would discover them anyway, and get "jollies" about the discovery.
So, they tell you that the registers exist, and they tell you not to use them.
So don't use them.  


0 件の賞賛
返信

1,025件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Divya on Wed Nov 06 04:43:02 MST 2013
Can anyone please answer?? Its been quite a while since I posted this question..
Isnt there any use of test registers?
0 件の賞賛
返信