Test registers of SPI module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Test registers of SPI module

1,352 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Divya on Mon Oct 28 02:17:30 MST 2013
What for SPI Test Status Register and SPI Test Control Registers are used in SPI module?
Please explain with scenario.
Thanks in advance.
Labels (1)
0 Kudos
Reply
2 Replies

1,341 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Wed Nov 06 16:47:26 MST 2013
from UM10503.pdf
Note that the bits in this register are intended for functional verification only. This register should not be used for normal operation.

most likely these are registers that are used for internal NXP testing
to test the peripheral.
they probably do not need to be mentioned in the manual, but some one would discover them anyway, and get "jollies" about the discovery.
So, they tell you that the registers exist, and they tell you not to use them.
So don't use them.  


0 Kudos
Reply

1,341 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Divya on Wed Nov 06 04:43:02 MST 2013
Can anyone please answer?? Its been quite a while since I posted this question..
Isnt there any use of test registers?
0 Kudos
Reply