Terminate, build and debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Terminate, build and debug

2,575 次查看
ianbenton
Senior Contributor I

I've recently upgraded to 11.1.1, and I note that the function called "terminate, build and debug" now only does "terminate and debug" even though it is still labelled "terminate, build and debug". I didn't see any information on this in the list of changes. How can I get it back to doing all three?

Also, I note that even when "debug" is selected it occasionally does "attach" instead. The only way I have found to reset it, is to select "erase flash via linkserver", erase the flash, then reselect "debug" and which point I get the dialogue box asking if I really want "debug" not "attach", and after that it works. Is there a better way?

标签 (4)
标记 (1)
0 项奖励
回复
1 回复

2,534 次查看
1234567890
Contributor IV

I'm not sure whether you mean 'Build (if required before launching' with 'build':

pastedImage_1.png

Same about the second part ('attach'): The short solution would be to delete the launch configuration and then create a new one. Maybe untick 'attach' on the Debugger Tab of your launch configuration (depends on your debugger...).

0 项奖励
回复