Terminate, build and debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Terminate, build and debug

2,524件の閲覧回数
ianbenton
Senior Contributor I

I've recently upgraded to 11.1.1, and I note that the function called "terminate, build and debug" now only does "terminate and debug" even though it is still labelled "terminate, build and debug". I didn't see any information on this in the list of changes. How can I get it back to doing all three?

Also, I note that even when "debug" is selected it occasionally does "attach" instead. The only way I have found to reset it, is to select "erase flash via linkserver", erase the flash, then reselect "debug" and which point I get the dialogue box asking if I really want "debug" not "attach", and after that it works. Is there a better way?

ラベル(4)
タグ(1)
0 件の賞賛
返信
1 返信

2,483件の閲覧回数
1234567890
Contributor IV

I'm not sure whether you mean 'Build (if required before launching' with 'build':

pastedImage_1.png

Same about the second part ('attach'): The short solution would be to delete the launch configuration and then create a new one. Maybe untick 'attach' on the Debugger Tab of your launch configuration (depends on your debugger...).

0 件の賞賛
返信