Targetboard CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Targetboard CAN

2,588 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Analog2Can on Tue May 27 12:02:30 MST 2014
Hello,
I programmed a LPC11C24 to read analog ports and send the values via CAN. Everthing worked fine. Now I cut the board and wanted to use just the Target board. I supply it with 5V and 3.3V, but now CAN isn't working. Do I have to enable something?
Labels (1)
0 Kudos
Reply
3 Replies

2,578 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue May 27 12:40:50 MST 2014

Quote: Analog2Can
Whats about J4-18?



Believe it or not, LPC11C24 requires a 5V supply voltage for its 5V CAN-transceiver at pin 20   :O  :quest:   :O

NXP has no 3.3V CAN-transceiver  :)

With connected LPC-link this is done by J4-18 as shown in schematic...
0 Kudos
Reply

2,575 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Analog2Can on Tue May 27 12:34:09 MST 2014
I connected it like this.

Whats about J4-18?
0 Kudos
Reply

2,575 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue May 27 12:13:15 MST 2014

Quote: Analog2Can
I supply it with 5V and 3.3V, but now CAN isn't working.



Where?

What about J4-18?
0 Kudos
Reply