State Configurable Timer on LPC1830 to measure input signal H,V?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

State Configurable Timer on LPC1830 to measure input signal H,V?

1,128件の閲覧回数
kensu
Contributor V

Dear Sirs,

I have a purpose to measure input signal H,V total clock (ex:  input signal with external H,V sync clock input).

Is it possible to use SCT counter to measure the H,V clock?

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

990件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ken Su,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

1) Is it possible to use SCT counter to measure the H,V clock?
Yes, of course.

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信