Spi configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Spi configuration

1,046 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Navneet Kaur on Mon Aug 24 10:18:05 MST 2015
Hi,

I am using LPC 54102 development board which I have connected to a rf reciever using digital ports (jumper 1) . I am using the example code - rom_spim_int to connect both MCU and the reciever using SPI. The problem that I am facing is that how do I make sure that the are connected correctly? What changes do I need to make for correct configuration ?

Kindly help.

Thanks
Navneet
Labels (1)
0 Kudos
Reply
0 Replies