Spi configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Spi configuration

1,061件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Navneet Kaur on Mon Aug 24 10:18:05 MST 2015
Hi,

I am using LPC 54102 development board which I have connected to a rf reciever using digital ports (jumper 1) . I am using the example code - rom_spim_int to connect both MCU and the reciever using SPI. The problem that I am facing is that how do I make sure that the are connected correctly? What changes do I need to make for correct configuration ?

Kindly help.

Thanks
Navneet
ラベル(1)
0 件の賞賛
返信
0 返答(返信)