[Solved] WDOSC not starting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Solved] WDOSC not starting

754件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Sun May 11 15:22:10 MST 2014
I want to run a LPC812 at WDOSC / n to get an idea of power consumption at low frequencies.
Since my program kept freezing, when switching the clock to WDOSC, I output WDOSC to CLKOUT.
Outcome: I can't get WDOSC running at all |(
What am I missing?

I configure it using WDOSCCTRL. I even switched on the WWDT bit in SYSAHBCLKCTRL which should not be needed in my opinion.
What else is needed for starting WDOSC?

SOLVED: I should search the manual using 'WD[color=#f03]T[/color]OSC  ;-)
ラベル(1)
0 件の賞賛
返信
0 返答(返信)