Software example for lpc43Sxx AES engine

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Software example for lpc43Sxx AES engine

2,485 Views
sylvio5
Contributor II

Hello

Is there any code snipet or application note or project example for how to use the hardware AES engin of the LPC43S serie ?

Thank you very much

Cheers

Labels (1)
0 Kudos
Reply
3 Replies

2,136 Views
sylvio5
Contributor II

Hello Soledad, thank you for your answer but as I see this application note refers to a library that doesn't use the hardware engine of the LPC43Sxx. What I would like to do is using this hardware engine. 

Is there any application note or code example for that ?

Regards

0 Kudos
Reply

2,136 Views
sylvio5
Contributor II

Is there really any example neither AN for using the hardware AES engine of LPC S series ???

0 Kudos
Reply

2,136 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the AN11241, this application note discusses an implementation of an AES encryption algorithm according to the FIPS197 standard.

http://cache.nxp.com/documents/application_note/AN11241.zip?fsrch=1&sr=1&pageNum=1 

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply