Sleep mode dma wake up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sleep mode dma wake up

ソリューションへジャンプ
1,562件の閲覧回数
ujwal_kumar_N_L
Contributor III

Hi community ,
I'm working on the Sleep modes of the NXP LPC55S69 board.
I'm trying to wake up the system using uart2 which is configurated as DMA will the DMA IRQ wake up the device or I need to Configure the Flexcomm as the Interrupt or the DMA irq will work ??
Device used LPC55S69
Sleep mode wake up using flexcomm2
Thank you and regards 
UJWAL

0 件の賞賛
返信
1 解決策
1,537件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ujwal_kumar_N_L 

Yes, need enable DMA interrupt before enter sleep mode, then  DMA interrupt will wake up cpu.

 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,538件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ujwal_kumar_N_L 

Yes, need enable DMA interrupt before enter sleep mode, then  DMA interrupt will wake up cpu.

 

BR

Alice

0 件の賞賛
返信