LPC4357 SD卡支持64G吗?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4357 SD卡支持64G吗?

1,436件の閲覧回数
lilipeeeee
Contributor I

你好!

       最近想使用大容量的存储空间,请问LPC4357 支持64G的SD卡吗?有什么方式可以扩展吗?具体实现方式是?

       期待你的回复!谢谢!

0 件の賞賛
返信
4 返答(返信)

1,395件の閲覧回数
CarrieDuoduo
Contributor I

.

Life-long learning
0 件の賞賛
返信

1,427件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @lilipeeeee 

Yes, it supports.

 

BR

Alice

0 件の賞賛
返信

1,397件の閲覧回数
lilipeeeee
Contributor I

LPC4357使用SD卡最大支持到多大?256G?128G?      支持64GSD卡,可直接在LPC4357上使用的文件系统吗?

0 件の賞賛
返信

1,354件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @lilipeeeee 

1) "LPC4357使用SD卡最大支持到多大?256G?128G?   

->> You need first confirm which SD card you want to use, then test, because for different manufacturers, SD card not the same.

2) There is SD card demo under lpcopen, you can refer to, download from:

https://www.nxp.com/design/design-center/software/software-library/lpcopen-software-development-plat...  

About Filesystem demo, you can find from arm, refer to thread:

https://community.nxp.com/t5/Processor-Expert-Software/LPC4357-Filesystem-demo/m-p/1431994  

 

 

BR

Alice

0 件の賞賛
返信