Sleep mode dma wake up

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Sleep mode dma wake up

跳至解决方案
1,592 次查看
ujwal_kumar_N_L
Contributor III

Hi community ,
I'm working on the Sleep modes of the NXP LPC55S69 board.
I'm trying to wake up the system using uart2 which is configurated as DMA will the DMA IRQ wake up the device or I need to Configure the Flexcomm as the Interrupt or the DMA irq will work ??
Device used LPC55S69
Sleep mode wake up using flexcomm2
Thank you and regards 
UJWAL

0 项奖励
回复
1 解答
1,567 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ujwal_kumar_N_L 

Yes, need enable DMA interrupt before enter sleep mode, then  DMA interrupt will wake up cpu.

 

BR

Alice

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,568 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ujwal_kumar_N_L 

Yes, need enable DMA interrupt before enter sleep mode, then  DMA interrupt will wake up cpu.

 

BR

Alice

0 项奖励
回复