Size of MCUXPRESSO icon

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Size of MCUXPRESSO icon

2,619 Views
Y_INO
Contributor I

小さなMCUXPRESSOアイコンを改善する方法はありますか?

0 Kudos
Reply
4 Replies

2,610 Views
frank_m
Senior Contributor III

My guess about the ideographs being Japanese being correct, it seems.
I had to use a machine translator, I don't speak or read any Japanese.

But icon sizes are a system setting, and not under control of individual applications.
Just right-click on the desktop, select "View", and there "medium icons" or "large icons".

0 Kudos
Reply

2,591 Views
Y_INO
Contributor I

Thank you for your response to my question.Is it possible to change the size of the IDE toolbar icons from the default size? They seem too small and I find it difficult to operate.

0 Kudos
Reply

2,582 Views
ErichStyger
Specialist I

Hi @Y_INO ,

yes, you can change the toolbar icon size with changing the DPI settings, see https://mcuoneclipse.com/2017/10/11/dealing-with-eclipse-and-very-small-icons-on-ultra-high-density-...

I hope this helps,

Erich

0 Kudos
Reply

2,563 Views
Y_INO
Contributor I

ありがとうございました。アイコンが拡大されました。

0 Kudos
Reply