Shall we enable BOD reset always?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Shall we enable BOD reset always?

1,111件の閲覧回数
Sun1998
Contributor I

Recently we met a case that the code is lost during power on/off cycle on another brand MCU, this issue was solved by enabled BOD reset feature. 

For LPC11xx series, I wonder,  shall we must enable BOD reset? if without it, is there any risk losing the programmed code in flash?

PS: no IAP usage in this case, the FLASH is used as code ROM only. 

0 件の賞賛
返信
1 返信

1,098件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

BOD is used to prevent the circuit when the voltage drops unexpectedly for a very short time so as to avoid failure. 

Whether or not to enable BOD depends on your external power supply circuit stability. LPC11xx has BOD. We can enable it if need.

Hope this helps,

Jun Zhang 

 

0 件の賞賛
返信