LPC55s16 seems to fit my need I have questions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55s16 seems to fit my need I have questions

Jump to solution
2,100 Views
sam_m
Contributor II

So I came across this part because it has SW security.  I got here because of the Raspberry Pi Pico, I tinkered and made some stuff with it.  Now I want to use this device as the main and the Pico in support.  The Pico is setup to be simple to "execute" grab a USB cable and write some python.  Alot of the primitives are taken care of for interfaces and gpio.

Pico has one of these, another Pico can be made to be a Probe.  Is this possible?  Pico only use CLK and DIO, ground. Pico have USB as their main interface the SWD is extra goodness and not super necessary but helpful.  

If I get the MCU link and not a dev board, can I just hook the SWD pins to pins and debug?  Meaning I make my own board and provide the interface as the device seems to very easily stand alone.  What are the necessary pins?  

Is in MCU link the most likely way I can program an uninitialized device?  I cannot use any of the current interfaces?  I know there is some type of ROM that may have primordial flashing routines, as it is mentioned a UART interface can.  I haven't looked hard for the SW user guide for the device which may answer some of this.

If I use the IDE and USB instead will anything happen(my guess is no as Pico has that boot as USB flash drive and a way to load a file that will allow interaction with python or c or whatever.)?  

I did create an IDE for what I thought I would need as a bare board, but first thought I might by a dev board and then decided MCU link might be enough.

So the general question is, if I plop the device on a board and provide some pins/connections can I make it work with the IDE and some interface without the need for the dev board for my "training"?

0 Kudos
Reply
1 Solution
2,026 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @sam_m,

Yes, the MCU Link should be enough for your needs by utilizing SWD. If you have any other doubts about documentation or guidelines, don't hesitate to ask.

Best regards, Julian

View solution in original post

4 Replies
2,075 Views
sam_m
Contributor II
hey 
 
this is super helpful!  I actually had the third document.
 
from what i gather looking at the user manual for the part i can rely on SWD interface to begin a project in the software domain,  and eventually graduate it to say usb input of application code. but that is not necessary?  i can do all load and debug thru swd near term?  including setting up secure code methods?  (challenge and response and all that)
 
i then should use your MCU link for easiest best results?  (it is not expensive enough to create other problems with some other method, like I had suggested with Pico probe) I have it's UM as well.
 
There is no mention of the benefits of SWO but I gather there is and I planned to use it.
 
All of these help me establish a base line for the design as for now I just have it mocked up for my application in schematic tools.  It is a super dense thing but the datasheet is only about half the information as all of the above and other things are needed to start feeling secure in the design particulars.  I think it is not obvious from the web site how to piece things together. 
 
The device UM11295.pdf has been very useful.
 
But this reply is reasonably fast and reassuring!
 
thanks
0 Kudos
Reply
2,027 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @sam_m,

Yes, the MCU Link should be enough for your needs by utilizing SWD. If you have any other doubts about documentation or guidelines, don't hesitate to ask.

Best regards, Julian

2,021 Views
sam_m
Contributor II

Ok, sorry for the double check but in the UM11295 for the device is section 51.6.1 and while describing explicitly what happens does sound a little worrisome when a person has no experience with this part.  However I am very comfortable that the MCU-link handles all of this easily, I assume.  

I also assume that the MCU-link can establish SWO functionality as well.

I very likely will just design this part in on my circuit and not get the dev board, so I need to be comfortable with this vital method for code development.  The dev board may not be this "low of a state" so it will not provide the verification of the functions.

2,078 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @sam_m,

MCU Link is enough to program the stand-alone CPU. If you need recommendations for debugging the CPU you will find this post useful for necessary pins: Design Considerations for Debug - NXP Community.

You can base your design on the hardware recommendation guidelines of the 55s16 in the application note and the schematics in its page:

I hope you find this useful.

Best regards, Julian