Setup LPC824 in a multimaster situation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setup LPC824 in a multimaster situation

2,034件の閲覧回数
azellen
Contributor I

I have two LPC824 and two other nrf51822 micro controllers charing the same I2C bus.

All need to be master at some point, on the LPC824 I am running hardware I2C, and on the nrf51822 I am running sw I2C, so the bus speed is really slow.

I have an issue when the two nrf51822 is communicating on the bus, the LPC824 is hijacking the bus in the middle of the communication, when the software want to take control of the bus.

Do I need to take any precautions before I put the LPC824 into master and issue the START condition.

I have set up the LPC824 like this

Chip_Clock_EnablePeiphClock(SYSCTL_CLOCK_I2C0);
Chip_SYSCTL_PeriphReset(RESET_I2C0);

LPC_I2C0->CFG = I2C_CFG_SLVEN;

LPC_I2C_SLVADR[0] = 0x80;

LPC_I2C_SLVADR[1] = 0x82;

LPC_I2C0->INTENSET = I2C_INTENSET_SLVPENDING | I2C_INTENSET_SLVDESEL;

NVIC_EnableIRQ(I2C0_IRQn);

When the micrcontroller need to transmit data, I have the following code

u8 setupMaster(u8 address) {

if((LPC_I2C0->STAT >> 8 ) & 0x40) {   //Check if the SLAVESEL bit is set

   return false;

}

SPI0_SEND_8bit(address);

SPI0_WAIT_FOR_FRAME();

SPI0_SEND_16bit_EOT(LPC_I2C0->STAT);

NVIC_DisableIRQ(I2C0_IRQn);

LPC_I2C0->CFG = I2C_CFG_MSTEN;

LPC_I2C0->CLKDIV = 100;

LPC_I2C0->MSTTIME = (3 << 4) | ( 3 << 0);

LPC_I2C0->INTENSET = I2C_INTENSET_MSTPENDING | I2C_INTENSET_MSTRARBLOSS;

LPC_I2C0->STAT = I2C_STAT_MSTSTSTPERR | I2C_STAT_MSTRARBLOSS | I2C_STAT_MSTPENDING | I2C_STAT_SLVDESEL  | I2C_STAT_MONOV | I2C_STAT_MONIDLE | I2C_STAT_EVENTTIMEOUT;

NVIC_ClearPendingIRQ(I2C0_IRQn);

LPC_I2C0->MSTDAT = address;

LPC_I2C0->MSTCTL = I2C_MSTCTL_MSTSTART;

NVIC_EnableIRQ(I2C0_IRQn);

return true;

}

When this is executed (I have some debug output on the SPI to know when it is happening, there is sometimes a distrubence in the I2C transmission that is ongoing, it could be that the CLK is hold down, that a start condition is issued and so on, so the question is.

When I use the LPC824 in an multimaster situation, how should I set it up to be sure that it leave ongoing I2C transmissions alone and wait until they are completed, is there any constrains about the I2C speed from the other masters to operate well?

/Anders Zellén

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,798件の閲覧回数
azellen
Contributor I

I have found out that the multimaster feature is functional, if the master and slave is Active all the time

(LPC_I2C->CFG = I2C_CFG_MSTEN | I2C_CFG_SLVEN)

When the device start a transmission, I enable the master pending and master arbitration loss interrupts

(LPC_I2C0->INTENSET = I2C_INTENSET_MSTPENDING | I2C_INTENSET_MSTRARBLOSS)

In the interrupt handler, I check for the I2C_STAT_MSTPENDING flag in LPC_I2C0->STAT and that the Master pending and master arbitration loss interrupts are enabled


As soon as the master transmit is completed, I disable the master pending and master arbitration loss interrupts.

That is becouse the I2C_STAT_MSTPENDING is Always Active when the master is idle, so that part of the interrupt routine should have been executed each time a slave interrupt need to be served.

/Anders Zellén

0 件の賞賛
返信

1,798件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Anders,

Your approach is correct, you can enable the master from the beginning and before starting the transmission make sure that the master state is idle, this will prevent that the master takes control of the bus when there is an ongoing transmission on the bus.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信