Sample/Library code for storing configuration parameters in FLASH Memory area?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sample/Library code for storing configuration parameters in FLASH Memory area?

932 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nasuos on Fri Nov 22 14:39:50 MST 2013
Is there any Sample code or library for storing configuration parameters in the FLASH Memory area?  I know I could write it myself with managing the area myself but thought I would check first to see if any examples exist?  That is I want to store user configurable data in a section of the FLASH memory.  Be nice to if there was sample code that also encapsulated it in a CRC or checksum for corruption checking and maybe a dual system with primary/backup section.

Thanks.
标签 (1)
0 项奖励
回复
0 回复数