Sample/Library code for storing configuration parameters in FLASH Memory area?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sample/Library code for storing configuration parameters in FLASH Memory area?

941 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nasuos on Fri Nov 22 14:39:50 MST 2013
Is there any Sample code or library for storing configuration parameters in the FLASH Memory area?  I know I could write it myself with managing the area myself but thought I would check first to see if any examples exist?  That is I want to store user configurable data in a section of the FLASH memory.  Be nice to if there was sample code that also encapsulated it in a CRC or checksum for corruption checking and maybe a dual system with primary/backup section.

Thanks.
Labels (1)
0 Kudos
Reply
0 Replies