Sample/Library code for storing configuration parameters in FLASH Memory area?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sample/Library code for storing configuration parameters in FLASH Memory area?

935件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nasuos on Fri Nov 22 14:39:50 MST 2013
Is there any Sample code or library for storing configuration parameters in the FLASH Memory area?  I know I could write it myself with managing the area myself but thought I would check first to see if any examples exist?  That is I want to store user configurable data in a section of the FLASH memory.  Be nice to if there was sample code that also encapsulated it in a CRC or checksum for corruption checking and maybe a dual system with primary/backup section.

Thanks.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)