SWDIO short with ground

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SWDIO short with ground

3,796件の閲覧回数
NVazquez
Contributor IV

We are working on a custom board with LPC54S016 controller.  We have 3 boards, 2 of them we cannot program, it has SWDIO pin short with ground. The schematic is pretty straight forward. One of the board worked for 2hours and then stopped working(I couldn't program same reason short between SWDIO and ground). I am using ULINK2 debugger. We have a 5v voltage regulator which then supplies 3.3v.

 

Is there any reason that could cause the short between the SWDIO and ground?  

 

NVazquez_0-1661985702161.png

NVazquez_1-1661985751125.png

 

0 件の賞賛
返信
3 返答(返信)

3,788件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Neha

I think the SWD connector is correct from the pin assignment and pull-up resistor, how do you know that the SWDIO pin is shorten with GND?

Anyway, pls note that you have to use 3.3V logic for the SWD signals.

BR

XiangJun Rong

タグ(1)
0 件の賞賛
返信

3,783件の閲覧回数
NVazquez
Contributor IV

We checked on the multimeter. We took the pull up, desoldered that pin and it was still short with ground.

タグ(1)
0 件の賞賛
返信

3,776件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you float the SWDIO pin, which means that the pin is NO connection, I suppose that the SWDIO pin is an input pin, in the case, if you connect a pull-up resistor, you can get high logic voltage. If you can not get high voltage but get LOW logic voltage, I suppose that there are two cases, the SWDIO pin is in output mode and output low logic voltage, another case is that the SWDIO pin is damaged, shorten to GND internally.

The SWDIO is an input/output pin, it can output data and input data.

Pls connect the debugger probe to the SWD port and check the SWDIO pin waveform with a scope during downloading process.

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信