SVD peripheral file file LPC5528

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SVD peripheral file file LPC5528

ソリューションへジャンプ
4,695件の閲覧回数
chetferry
Contributor II

I am debugging a product with an LPC5528 mcu.  McuExpresso seems to know about the peripheral registers.  I need to debug in Ozone and have a Cmake based project.  Can someone help me locate the .svd file for this part?  I have hunted through the SDK files and also the mcuxpresso install area where I did create a hello world project for my target which worked fine.  I am on MacOs.  Thanks.

 

 

0 件の賞賛
返信
1 解決策
4,691件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello chetferry,

 

The SVD file is present in SDK, while it is not using *.svd extension. it is *.xml,

SDK_2.9.1_LPCXpresso55S28\devices\LPC55S28

Alice_Yang_0-1630050505662.png

 

BR

Alice

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,691件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello chetferry,

 

The SVD file is present in SDK, while it is not using *.svd extension. it is *.xml,

SDK_2.9.1_LPCXpresso55S28\devices\LPC55S28

Alice_Yang_0-1630050505662.png

 

BR

Alice

 

 

0 件の賞賛
返信
3,681件の閲覧回数
AgustinOrdonez
Contributor I

Can this file be renamed to .svd extension to use it as such or does it need a conversion?

0 件の賞賛
返信
3,665件の閲覧回数
ErichStyger
Specialist I

just rename it, no conversion needed.

0 件の賞賛
返信
4,686件の閲覧回数
chetferry
Contributor II

Thank you.  Thats exactly what I needed

 

0 件の賞賛
返信