SPIFI and SPI in LPC4370

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPIFI and SPI in LPC4370

3,063 Views
hmyoong
Contributor III

LPC4370 is a flashless part with SPIFI and SPI peripehrals sharing similar pins.  It is necessary to use SPIFI to access external flash. Hence, the part could not external SPI devices (such as ATMEL ATWINC1500) . Do you have suggestion? 

SPI interface in ATWINC1500 is for host interface and UART interface is for debug.

Thanks.

Labels (1)
Tags (3)
3 Replies

2,719 Views
hmyoong
Contributor III

Thanks. I can use ssp1.

0 Kudos
Reply

2,719 Views
jeremyzhou
NXP Employee
NXP Employee

Hi HM Yoong,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

In the LPC43xx, the SSP0/1 and SPI module both are able to interface external SPI device.

You can learn the more information in these chapters.

pastedImage_1.png

Have a great day.

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,719 Views
hmyoong
Contributor III

I checked again, SPIFI has a #SPIFI_CS pin.  Has anyone try to use SPIFI/SPI with external flash and other devices, multiplexing external devices using CS pins?

Of course, program in the flash (assuming not too big) is transferred to internal RAM.

0 Kudos
Reply