SPI troubles

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI troubles

1,150 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Scribe on Tue Jun 18 05:27:29 MST 2013

Hi guys,


I've written some simple SPI code using Keil, however I'm unable to get the module to transmit and trigger the SPI tranfer complete interrupt flag. Am I missing anything from the following code?


<div>#define  CMSIS_BITPOSITIONS 1</div>
<div>#include &lt;LPC43xx.h&gt;</div>
<div>int main( void )</div>
<div>{</div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>// Update the System Core Clock</div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>SystemCoreClockUpdate();</div>
<div> </div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>// Configure pins for SPI</div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>LPC_SCU-&gt;SFSP3_6 = 1; // MISO</div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>LPC_SCU-&gt;SFSP3_7 = 1; // MOSI</div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>LPC_SCU-&gt;SFSP3_3 = 1; // SCK</div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>LPC_SCU-&gt;SFSP3_8 = 1; // SSEL</div>
<div> </div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>// Configure the SPI Master Clock (PCLK_SPI / SPCCR)</div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>LPC_SPI-&gt;CCR = 16;</div>
<div> </div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>// Configure the SPI Module for Master Mode and X</div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>LPC_SPI-&gt;CR |= SPI_CR_MSTR_Msk | SPI_CR_SPIE_Msk;</div>
<div> </div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>while( 1 )</div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>{</div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>LPC_SPI-&gt;DR = 0xA1;</div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>while( !(LPC_SPI-&gt;SR &amp; SPI_SR_SPIF_Msk) );</div>
<div><span class="Apple-tab-span" style="white-space: pre;"> </span>}</div>
<div>}</div>
<div><span style="font-family: Verdana, Arial, Helvetica, sans-serif;">Many thanks</span></div>
标签 (1)
0 项奖励
回复
1 回复

1,116 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wmues on Tue Jun 18 13:15:08 MST 2013

Setup Power Managment - SPI clock enabled?

0 项奖励
回复