SPI clock mode 0 polarity wrong (inverted)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI clock mode 0 polarity wrong (inverted)

ソリューションへジャンプ
6,077件の閲覧回数
simonwyss
Contributor III

While testing the SPI clock modes I measured the following graphs with my logic analyzer:

SPI clock mode 0:

pastedImage_1.png

SPI clock mode 1:

pastedImage_2.png

SPI clock mode 2:

pastedImage_3.png

SPI clock mode 3:

pastedImage_4.png

My SPI settings:
Master Mode
MSB first
Data Length: 8 Bit

I used no high level functions to start the transfer.

The code used is mainly from the periph_spi_sm_int example in the LPCopen lib.

#define LPC_SPIMASTERPORT                   LPC_SPI1

static void setupSPIMaster(void)
{
     SPI_CFGSETUP_T spiSetup;
     //SPIM_DELAY_CONFIG_T masterDelay;

     /* Initialize SPI controller */
     Chip_SPI_Init(LPC_SPIMASTERPORT);

     /* Call to initialize first SPI controller for mode0, master mode,
        MSB first */
     Chip_SPI_Enable(LPC_SPIMASTERPORT);
     spiSetup.master = 1;
     spiSetup.lsbFirst = 0; //0=MSB first
     spiSetup.mode = SPI_CLOCK_MODE3;
     Chip_SPI_ConfigureSPI(LPC_SPIMASTERPORT, &spiSetup);

     /* Setup master controller SSEL0 for active low select */
     //Chip_SPI_SetCSPolLow(LPC_SPIMASTERPORT, 0);

     /* Setup master clock rate, slave clock doesn't need to be setup */
     Chip_SPIM_SetClockRate(LPC_SPIMASTERPORT, LPCMASTERCLOCKRATE);

     //set SPI transmit length to 8 bit
     Chip_SPI_SetXferSize(LPC_SPIMASTERPORT, 8);
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

To write a byte out by SPI I used the following code:

//write single byte to SPI1
while(!(Chip_SPI_GetStatus(LPC_SPI1) & (SPI_STAT_TXRDY) ) ); //wait until ready to transmit
Chip_SPI_WriteTXData(LPC_SPI1, 0x02);  //write 0x02 to SPI1
          
//read single byte from SPI1
while((Chip_SPI_GetStatus(LPC_SPI1) & (SPI_STAT_RXRDY) ) ); //wait until one byte received
spiValue =  Chip_SPI_ReadRXData(LPC_SPI1);‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

In my opinion the SPI clock Mode 1 and 3 are correct working.

However the Mode 0 and 2 are not working correct.

In Mode 0 the clock should stay low in idle state and in Mode 2 it should stay high.

User manual UM10850 (LPC54102)

pastedImage_7.png

I set the slave select (chip select) by my selfe. I didn't want to use the slave select automatic. 

Did I configure something wrong?

ラベル(1)
1 解決策
5,124件の閲覧回数
simonwyss
Contributor III

Thank you for your reply.

The SPI clock modes seem to work as expected. My posted pictures of the signals are correct. 

Misleading was, that in clock mode 0 the clock stays high before the next byte starts. This happens due to "data stalls". The clock goes only low, if the next byte is ready to be transmitted. 

I coded a minimal example without the use of the high-level callbacks for SPI data transfer.

Description of the SPI module of this microcontroller:

If the SSEL Assert is enabled, the SSEL is pulled active (low) if a data byte is written out on SPI. Additional bytes can be written the same way.

- If you know the when the last byte is sent, you can set the "end of transfer" bit (EOT in the TXCTL register). Then the SSEL is deactivated (high) after the transmission of the last byte.

-If you don't know when the last byte is sent, you can later force the SSEL to be pulled low by setting the "END TRANSFER" bit (END TRANSFER in STAT register).

If you force the "END TRANSFER" you have to wait until the SSEL is deassert (watch on "slave select deassert" bit in STAT register).

Result of the example:

pastedImage_1.png

The example project (LPCXpresso) is attached at the end of this post.

Source Code: 

/*
 * @brief SPI Example for LPC54102  (taken from LPCopen periph_spi_sm_int example)
 *
 * @note
 * Copyright(C) NXP Semiconductors, 2014
 * All rights reserved.
 *
 * @note
 * Copyright(C) Simon Wyss, 2017
 * Mail: blog (at) simonwyss.com
 *
 * @par
 * Software that is described herein is for illustrative purposes only
 * which provides customers with programming information regarding the
 * LPC products.  This software is supplied "AS IS" without any warranties of
 * any kind, and NXP Semiconductors and its licensor disclaim any and
 * all warranties, express or implied, including all implied warranties of
 * merchantability, fitness for a particular purpose and non-infringement of
 * intellectual property rights.  NXP Semiconductors assumes no responsibility
 * or liability for the use of the software, conveys no license or rights under any
 * patent, copyright, mask work right, or any other intellectual property rights in
 * or to any products. NXP Semiconductors reserves the right to make changes
 * in the software without notification. NXP Semiconductors also makes no
 * representation or warranty that such application will be suitable for the
 * specified use without further testing or modification.
 *
 * @par
 * Permission to use, copy, modify, and distribute this software and its
 * documentation is hereby granted, under NXP Semiconductors' and its
 * licensor's relevant copyrights in the software, without fee, provided that it
 * is used in conjunction with NXP Semiconductors microcontrollers.  This
 * copyright, permission, and disclaimer notice must appear in all copies of
 * this code.
 *
 *
 *
 */

#include "board.h"


/*****************************************************************************
 * Private types/enumerations/variables
 ****************************************************************************/
#define LOW    0
#define HIGH   1
#define OUTPUT 1
#define INPUT  0

/*****************************************************************************
 * Public types/enumerations/variables
 ****************************************************************************/

/* Board specific example setup */
#define LPC_SPIMASTERPORT                   LPC_SPI1

#define LPCMASTERCLOCKRATE                   10000 //10kHz for Debug (4000000)

/*****************************************************************************
 * Private functions
 ****************************************************************************/
/* Initializes pin muxing for SPI1 interface - note that SystemInit() may
   already setup your pin muxing at system startup */
static void Init_SPI_PinMux(void)
{
#if defined(BOARD_NXP_LPCXPRESSO_54102)
     /* SPI1 (master) */
     Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 6,  (IOCON_FUNC2 | IOCON_MODE_PULLUP | IOCON_DIGITAL_EN));     /* SPI1_SCK */
     Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 7,  (IOCON_FUNC2 | IOCON_MODE_PULLUP | IOCON_DIGITAL_EN));     /* SPI1_MOSI */
     Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 14, (IOCON_FUNC4 | IOCON_MODE_PULLUP | IOCON_DIGITAL_EN));     /* SPI1_MISO */
     Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 15, (IOCON_FUNC4 | IOCON_MODE_PULLUP | IOCON_DIGITAL_EN));     // GPIO CS for RFM95, FUNC4 for SSL
#else
     #warning    "Board pin muxing not available!"
#endif
}



static void setupSPIMaster(void)
{
     SPI_CFGSETUP_T spiSetup;
     //SPIM_DELAY_CONFIG_T masterDelay;

     /* Initialize SPI controller */
     Chip_SPI_Init(LPC_SPIMASTERPORT);

     /* Call to initialize first SPI controller for mode0, master mode,
        MSB first */
     Chip_SPI_Enable(LPC_SPIMASTERPORT);
     spiSetup.master = 1;
     spiSetup.lsbFirst = 0; //0=MSB first
     spiSetup.mode = SPI_CLOCK_MODE0;
     Chip_SPI_ConfigureSPI(LPC_SPIMASTERPORT, &spiSetup);
     //pSPI->TXCTRL = SPI_TXDATCTL_DEASSERT_ALL; //configured in Chip_SPI_ConfigureSPI

     /* Setup master controller SSEL0 for active low select */
     Chip_SPI_SetCSPolLow(LPC_SPIMASTERPORT, 0);

     /* Setup master clock rate, slave clock doesn't need to be setup */
     Chip_SPIM_SetClockRate(LPC_SPIMASTERPORT, LPCMASTERCLOCKRATE);

     //masterDelay.PreDelay = 0xD;
     //masterDelay.PostDelay = 0xD;
     //masterDelay.FrameDelay = 0xD;
     //masterDelay.TransferDelay = 0xD;
     //Chip_SPIM_DelayConfig(LPC_SPIMASTERPORT, &masterDelay); //delay unused when CS is forced low by the user

     //set SPI transmit length to 8 bit
     Chip_SPI_SetXferSize(LPC_SPIMASTERPORT, 8);

     Chip_SPIM_AssertSSEL(LPC_SPIMASTERPORT, 0);

     //SPI interrupts not used
     /* For the SPI controller configured in master mode, enable SPI master interrupts
        for interrupt service. Do not enable SPI_INTENSET_TXDYEN. */

     //Chip_SPI_EnableInts(LPC_SPIMASTERPORT, (SPI_INTENSET_RXDYEN | SPI_INTENSET_RXOVEN | SPI_INTENSET_TXUREN | SPI_INTENSET_SSAEN |
     //                                                  SPI_INTENSET_SSDEN));
     //Chip_SPIM_AssertSSEL(LPC_SPIMASTERPORT, 0);
     //Chip_SPIM_DeAssertSSEL(LPC_SPIMASTERPORT, 0);
}


/*****************************************************************************
 * Public functions
 ****************************************************************************/

uint8_t SPI_write(uint8_t spi_tx){
     //write single byte to SPI1
     while(!(Chip_SPI_GetStatus(LPC_SPI1) & (SPI_STAT_TXRDY) ) ); //wait until TX buffer empty
     Chip_SPI_WriteTXData(LPC_SPI1, spi_tx);

     //read single byte from SPI1
     while(!(Chip_SPI_GetStatus(LPC_SPI1) & (SPI_STAT_RXRDY) ) ); //wait until RX buffer full
     return Chip_SPI_ReadRXData(LPC_SPI1);
}

/* main function (C entry point) */
int main(void)
{
     /****   Define local variables for the application  ***/
     uint32_t Cnt;

     int loop = 1;     /* Used to avoid unreachable statement warning */
     /* Generic Initialization */
     SystemCoreClockUpdate();

     /* Board_Init calls Chip_GPIO_Init and enables GPIO clock if needed,
        Chip_GPIO_Init is not called again */
     Board_Init(); //sets LED GPIO as output

     //setup SPI PinMux
     Init_SPI_PinMux();

     /* Setup SPI controllers */
     setupSPIMaster();


     //SSEL0 is asserted automatically before first byte is clocked out with SPI
     //SSEL0 goes LOW
     SPI_write(0x02);

     SPI_write(0x03);

     SPI_write(0x04);

     //force deassert of SSEL0
     Chip_SPIM_ForceEndOfTransfer(LPC_SPIMASTERPORT); //force End of Transfer -> SSEL should go HIGH
     while((Chip_SPI_GetStatus(LPC_SPIMASTERPORT) & SPI_STAT_SSD) == 0); //wait until SSEL is HIGH
     Chip_SPI_ClearStatus(LPC_SPIMASTERPORT, SPI_STAT_SSD | SPI_STAT_SSA); //clear SSD and SSA state, that next SSD can be detected in this function
     //clear of SSA Flag is not necessary for next "force deassert of SSEL0"
     //SSEL0 is HIGH

     //SSEL0 goes LOW
     SPI_write(0x05);

     SPI_write(0x06);

     SPI_write(0x07);

     Chip_SPIM_ForceEndOfTransfer(LPC_SPIMASTERPORT);
     while((Chip_SPI_GetStatus(LPC_SPIMASTERPORT) & SPI_STAT_SSD) == 0);
     Chip_SPI_ClearStatus(LPC_SPIMASTERPORT, SPI_STAT_SSD | SPI_STAT_SSA);
     //SSEL0 is HIGH

     //SSEL0 goes LOW ...
     SPI_write(0x08);

     SPI_write(0x09);

     Chip_SPIM_ForceEndOfTransfer(LPC_SPIMASTERPORT);
     while((Chip_SPI_GetStatus(LPC_SPIMASTERPORT) & SPI_STAT_SSD) == 0);
     Chip_SPI_ClearStatus(LPC_SPIMASTERPORT, SPI_STAT_SSD | SPI_STAT_SSA);


     //repeat SPI write
     while (loop) {

          Board_LED_Toggle(0); //blink LED

          for (Cnt = 0; Cnt < (BOARD_MAINCLOCKRATE / 50); Cnt++) __NOP(); //wait some time (approximate 0.2 seconds)

          //SPI write
          SPI_write(0x0A);

          SPI_write(0x0B);

          //force deassert of SSEL0
          Chip_SPIM_ForceEndOfTransfer(LPC_SPIMASTERPORT);
          while((Chip_SPI_GetStatus(LPC_SPIMASTERPORT) & SPI_STAT_SSD) == 0);
          Chip_SPI_ClearStatus(LPC_SPIMASTERPORT, SPI_STAT_SSD | SPI_STAT_SSA);
     }

     return 0;
}
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,124件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Simon Wyss,

   What the code you are testing?

 I have test this code:lpc5410x_xpresso54102_keil_iar_v3.03.000_16\lpc5410x\prj_xpresso54102\iar\periph_spi_int

Download link:

http://www.nxp.com/assets/downloads/data/en/software/lpc5410x_xpresso54102_keil_iar_v3.03.000_16.zip 

board is lpcxpresso lpc54102

1. mode 0:

pastedImage_5.png

pastedImage_6.png

2.mode 1

pastedImage_7.png

pastedImage_8.png

3.mode 2:

pastedImage_2.png

wave:

pastedImage_3.png

4. mode 3

pastedImage_9.png

pastedImage_10.png

Compare with user manual:

It totally meets the demand.

You can test the same project as me on your side again.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

5,125件の閲覧回数
simonwyss
Contributor III

Thank you for your reply.

The SPI clock modes seem to work as expected. My posted pictures of the signals are correct. 

Misleading was, that in clock mode 0 the clock stays high before the next byte starts. This happens due to "data stalls". The clock goes only low, if the next byte is ready to be transmitted. 

I coded a minimal example without the use of the high-level callbacks for SPI data transfer.

Description of the SPI module of this microcontroller:

If the SSEL Assert is enabled, the SSEL is pulled active (low) if a data byte is written out on SPI. Additional bytes can be written the same way.

- If you know the when the last byte is sent, you can set the "end of transfer" bit (EOT in the TXCTL register). Then the SSEL is deactivated (high) after the transmission of the last byte.

-If you don't know when the last byte is sent, you can later force the SSEL to be pulled low by setting the "END TRANSFER" bit (END TRANSFER in STAT register).

If you force the "END TRANSFER" you have to wait until the SSEL is deassert (watch on "slave select deassert" bit in STAT register).

Result of the example:

pastedImage_1.png

The example project (LPCXpresso) is attached at the end of this post.

Source Code: 

/*
 * @brief SPI Example for LPC54102  (taken from LPCopen periph_spi_sm_int example)
 *
 * @note
 * Copyright(C) NXP Semiconductors, 2014
 * All rights reserved.
 *
 * @note
 * Copyright(C) Simon Wyss, 2017
 * Mail: blog (at) simonwyss.com
 *
 * @par
 * Software that is described herein is for illustrative purposes only
 * which provides customers with programming information regarding the
 * LPC products.  This software is supplied "AS IS" without any warranties of
 * any kind, and NXP Semiconductors and its licensor disclaim any and
 * all warranties, express or implied, including all implied warranties of
 * merchantability, fitness for a particular purpose and non-infringement of
 * intellectual property rights.  NXP Semiconductors assumes no responsibility
 * or liability for the use of the software, conveys no license or rights under any
 * patent, copyright, mask work right, or any other intellectual property rights in
 * or to any products. NXP Semiconductors reserves the right to make changes
 * in the software without notification. NXP Semiconductors also makes no
 * representation or warranty that such application will be suitable for the
 * specified use without further testing or modification.
 *
 * @par
 * Permission to use, copy, modify, and distribute this software and its
 * documentation is hereby granted, under NXP Semiconductors' and its
 * licensor's relevant copyrights in the software, without fee, provided that it
 * is used in conjunction with NXP Semiconductors microcontrollers.  This
 * copyright, permission, and disclaimer notice must appear in all copies of
 * this code.
 *
 *
 *
 */

#include "board.h"


/*****************************************************************************
 * Private types/enumerations/variables
 ****************************************************************************/
#define LOW    0
#define HIGH   1
#define OUTPUT 1
#define INPUT  0

/*****************************************************************************
 * Public types/enumerations/variables
 ****************************************************************************/

/* Board specific example setup */
#define LPC_SPIMASTERPORT                   LPC_SPI1

#define LPCMASTERCLOCKRATE                   10000 //10kHz for Debug (4000000)

/*****************************************************************************
 * Private functions
 ****************************************************************************/
/* Initializes pin muxing for SPI1 interface - note that SystemInit() may
   already setup your pin muxing at system startup */
static void Init_SPI_PinMux(void)
{
#if defined(BOARD_NXP_LPCXPRESSO_54102)
     /* SPI1 (master) */
     Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 6,  (IOCON_FUNC2 | IOCON_MODE_PULLUP | IOCON_DIGITAL_EN));     /* SPI1_SCK */
     Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 7,  (IOCON_FUNC2 | IOCON_MODE_PULLUP | IOCON_DIGITAL_EN));     /* SPI1_MOSI */
     Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 14, (IOCON_FUNC4 | IOCON_MODE_PULLUP | IOCON_DIGITAL_EN));     /* SPI1_MISO */
     Chip_IOCON_PinMuxSet(LPC_IOCON, 1, 15, (IOCON_FUNC4 | IOCON_MODE_PULLUP | IOCON_DIGITAL_EN));     // GPIO CS for RFM95, FUNC4 for SSL
#else
     #warning    "Board pin muxing not available!"
#endif
}



static void setupSPIMaster(void)
{
     SPI_CFGSETUP_T spiSetup;
     //SPIM_DELAY_CONFIG_T masterDelay;

     /* Initialize SPI controller */
     Chip_SPI_Init(LPC_SPIMASTERPORT);

     /* Call to initialize first SPI controller for mode0, master mode,
        MSB first */
     Chip_SPI_Enable(LPC_SPIMASTERPORT);
     spiSetup.master = 1;
     spiSetup.lsbFirst = 0; //0=MSB first
     spiSetup.mode = SPI_CLOCK_MODE0;
     Chip_SPI_ConfigureSPI(LPC_SPIMASTERPORT, &spiSetup);
     //pSPI->TXCTRL = SPI_TXDATCTL_DEASSERT_ALL; //configured in Chip_SPI_ConfigureSPI

     /* Setup master controller SSEL0 for active low select */
     Chip_SPI_SetCSPolLow(LPC_SPIMASTERPORT, 0);

     /* Setup master clock rate, slave clock doesn't need to be setup */
     Chip_SPIM_SetClockRate(LPC_SPIMASTERPORT, LPCMASTERCLOCKRATE);

     //masterDelay.PreDelay = 0xD;
     //masterDelay.PostDelay = 0xD;
     //masterDelay.FrameDelay = 0xD;
     //masterDelay.TransferDelay = 0xD;
     //Chip_SPIM_DelayConfig(LPC_SPIMASTERPORT, &masterDelay); //delay unused when CS is forced low by the user

     //set SPI transmit length to 8 bit
     Chip_SPI_SetXferSize(LPC_SPIMASTERPORT, 8);

     Chip_SPIM_AssertSSEL(LPC_SPIMASTERPORT, 0);

     //SPI interrupts not used
     /* For the SPI controller configured in master mode, enable SPI master interrupts
        for interrupt service. Do not enable SPI_INTENSET_TXDYEN. */

     //Chip_SPI_EnableInts(LPC_SPIMASTERPORT, (SPI_INTENSET_RXDYEN | SPI_INTENSET_RXOVEN | SPI_INTENSET_TXUREN | SPI_INTENSET_SSAEN |
     //                                                  SPI_INTENSET_SSDEN));
     //Chip_SPIM_AssertSSEL(LPC_SPIMASTERPORT, 0);
     //Chip_SPIM_DeAssertSSEL(LPC_SPIMASTERPORT, 0);
}


/*****************************************************************************
 * Public functions
 ****************************************************************************/

uint8_t SPI_write(uint8_t spi_tx){
     //write single byte to SPI1
     while(!(Chip_SPI_GetStatus(LPC_SPI1) & (SPI_STAT_TXRDY) ) ); //wait until TX buffer empty
     Chip_SPI_WriteTXData(LPC_SPI1, spi_tx);

     //read single byte from SPI1
     while(!(Chip_SPI_GetStatus(LPC_SPI1) & (SPI_STAT_RXRDY) ) ); //wait until RX buffer full
     return Chip_SPI_ReadRXData(LPC_SPI1);
}

/* main function (C entry point) */
int main(void)
{
     /****   Define local variables for the application  ***/
     uint32_t Cnt;

     int loop = 1;     /* Used to avoid unreachable statement warning */
     /* Generic Initialization */
     SystemCoreClockUpdate();

     /* Board_Init calls Chip_GPIO_Init and enables GPIO clock if needed,
        Chip_GPIO_Init is not called again */
     Board_Init(); //sets LED GPIO as output

     //setup SPI PinMux
     Init_SPI_PinMux();

     /* Setup SPI controllers */
     setupSPIMaster();


     //SSEL0 is asserted automatically before first byte is clocked out with SPI
     //SSEL0 goes LOW
     SPI_write(0x02);

     SPI_write(0x03);

     SPI_write(0x04);

     //force deassert of SSEL0
     Chip_SPIM_ForceEndOfTransfer(LPC_SPIMASTERPORT); //force End of Transfer -> SSEL should go HIGH
     while((Chip_SPI_GetStatus(LPC_SPIMASTERPORT) & SPI_STAT_SSD) == 0); //wait until SSEL is HIGH
     Chip_SPI_ClearStatus(LPC_SPIMASTERPORT, SPI_STAT_SSD | SPI_STAT_SSA); //clear SSD and SSA state, that next SSD can be detected in this function
     //clear of SSA Flag is not necessary for next "force deassert of SSEL0"
     //SSEL0 is HIGH

     //SSEL0 goes LOW
     SPI_write(0x05);

     SPI_write(0x06);

     SPI_write(0x07);

     Chip_SPIM_ForceEndOfTransfer(LPC_SPIMASTERPORT);
     while((Chip_SPI_GetStatus(LPC_SPIMASTERPORT) & SPI_STAT_SSD) == 0);
     Chip_SPI_ClearStatus(LPC_SPIMASTERPORT, SPI_STAT_SSD | SPI_STAT_SSA);
     //SSEL0 is HIGH

     //SSEL0 goes LOW ...
     SPI_write(0x08);

     SPI_write(0x09);

     Chip_SPIM_ForceEndOfTransfer(LPC_SPIMASTERPORT);
     while((Chip_SPI_GetStatus(LPC_SPIMASTERPORT) & SPI_STAT_SSD) == 0);
     Chip_SPI_ClearStatus(LPC_SPIMASTERPORT, SPI_STAT_SSD | SPI_STAT_SSA);


     //repeat SPI write
     while (loop) {

          Board_LED_Toggle(0); //blink LED

          for (Cnt = 0; Cnt < (BOARD_MAINCLOCKRATE / 50); Cnt++) __NOP(); //wait some time (approximate 0.2 seconds)

          //SPI write
          SPI_write(0x0A);

          SPI_write(0x0B);

          //force deassert of SSEL0
          Chip_SPIM_ForceEndOfTransfer(LPC_SPIMASTERPORT);
          while((Chip_SPI_GetStatus(LPC_SPIMASTERPORT) & SPI_STAT_SSD) == 0);
          Chip_SPI_ClearStatus(LPC_SPIMASTERPORT, SPI_STAT_SSD | SPI_STAT_SSA);
     }

     return 0;
}
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
0 件の賞賛
返信