SPI Slave select of LPC54102

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI Slave select of LPC54102

1,254 次查看
tejaljagdale
Contributor I

Hello,

I am using LPC54102  and I am trying to run example code from LPCopen library.  If I run example code as it is on may hardware it is working fine, but I if make changes in SSEL pin i.e Slave select pin it is not working as expected.

Please help me related same.

0 项奖励
回复
2 回复数

1,065 次查看
tejaljagdale
Contributor I

Thanks Victor, I'll try with SDK.

Tejal

0 项奖励
回复

1,065 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Tejal,

Are you using the example periph_spi_sm_int from the LPCopen or another one? 

What pin are you selecting when you make the change for the Slave select pin? 

The LPC54102 board has SDK, so I recommend you to use this instead of the LPCOpen, this because SDK is the newest software so all the new updates and bug fixes will come for SDK only. You can download it from here

I'll be waiting for your answer to continue with this problem!

Have a great day, 

Victor.

0 项奖励
回复