SPI COMMUNICATION ON LPC1768

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI COMMUNICATION ON LPC1768

4,254 次查看
akshaybuchake
Contributor I

I am doing communication in MCP3202 and LPC1768 via SPI(interrupt based) but i am getting data 0X00FF only....I am attaching code here

0 项奖励
回复
2 回复数

2,639 次查看
soledad
NXP Employee
NXP Employee

Hi,

In order to isolate the issue (hardware or software) could you please test the LPCopen spi examples?

LPCOpen Software for LPC17XX|NXP 

Have a great day,

Sol

 

 

 

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,639 次查看
akshaybuchake
Contributor I

Hello 

Thanks for early reply

But your solution to use NXP softwere  is not possible for me...because all the drivers other than SPI

I have to change according to that libraries....can you suggest the bug in my code?(for your verification of hardware one code with Memory card interfacing using SPI is working properly but ADC communication is not proper)... 

0 项奖励
回复