SDRAM vs SRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDRAM vs SRAM

1,604件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tomkulaga on Sat Feb 02 15:24:25 MST 2013
Would an SRAM greatly outperform an SDRAM for the lpc4337?

Not looking at capacity but purely at the time required to read a fixed number of bytes from a 200 Mhz SDRAM and a 10ns SRAM.

Thanks
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,561件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tomkulaga on Wed Feb 06 13:47:17 MST 2013
Thanks for that
0 件の賞賛
返信

1,561件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp21346 on Wed Feb 06 12:13:46 MST 2013
The synchronous bus used by the SDRAM is typically more efficient than the asynchronous bus used by SRAM. However, you have specified using a 10 ns SRAM which is very quick so it may be comparable. Also, SDRAM operation at 200 MHz is not supported on the LPC43xx (the maximum is 120 MHz).

-Dave @ NXP
0 件の賞賛
返信