SDRAM vs SRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDRAM vs SRAM

1,592 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tomkulaga on Sat Feb 02 15:24:25 MST 2013
Would an SRAM greatly outperform an SDRAM for the lpc4337?

Not looking at capacity but purely at the time required to read a fixed number of bytes from a 200 Mhz SDRAM and a 10ns SRAM.

Thanks
标签 (1)
0 项奖励
回复
2 回复数

1,549 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tomkulaga on Wed Feb 06 13:47:17 MST 2013
Thanks for that
0 项奖励
回复

1,549 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxp21346 on Wed Feb 06 12:13:46 MST 2013
The synchronous bus used by the SDRAM is typically more efficient than the asynchronous bus used by SRAM. However, you have specified using a 10 ns SRAM which is very quick so it may be comparable. Also, SDRAM operation at 200 MHz is not supported on the LPC43xx (the maximum is 120 MHz).

-Dave @ NXP
0 项奖励
回复