SDRAM Reference code for Understanding the functionality

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDRAM Reference code for Understanding the functionality

26,591 次查看
gauravmore
Contributor III

 Hi Jeremy, 

I am using LPC4367 controller with MCU Xpresso 10.3.0_2200. I am using SDRAM and NOR Flash interface in one of our projects. I was working with Evaluation board OM13088 but it that board no SDRAM and NOR flash interface is avialable.  I am using SDRAM and NOR flash both interfaced with EMC lines aviable in LPC4367 controller.

I refered the code in e lpcopen_3_02_lpcxpresso_mcb4357 and also refered periph_memtest and misc_spifi_tst demos. But there is no EMC init routine avialable. Is there any sample code or a reference code for SDRAM with proper intitiatilization routine.

Also i want to allocate one of my Buffer to SDRAM address, i got the information related to it i MCU expresso User guied but still i want to know than as we user 

__At(Address) attribute in Keil to allocate the array or a buffer like

uint16_t Buffer[1024]                     __at(0x28000000) 

In the similar manner how we can use it in MCU Expresso . I have  downloaded MCUxpresso 10.3.0 . 

To conclude i want the sample or areference code for SDRAM and NOR flash with proper EMC init routine which not provided in existing reference code

I need this since i want to test my development board which is ready. So please consider it on higher priority. Mean while i am trying to refere other forums as well for my understanding.

Thanks 

Gaurav More

标签 (2)
0 项奖励
回复
44 回复数

1,346 次查看
gauravmore
Contributor III

Hi Jeremy,

Sorry for the late response. As per  your inputs i have check the code for SDRAM available in LPCopen (periph_memtest) ans as per that I created new project for my development board using LPC4367 in LPCXpresso IDE

I am facing issue with the code where my code crashes in between.  Following the code for EMC initialization.

SDRAM which  i habe interface is "AS4C4M16SA-C&I"  64M – (4M x 16 bit) Synchronous DRAM (SDRAM). Controller is running at 100 Mhz.

#define EMC_ADDRESS_DYCS0   (0x28000000)

#define DRAM_SIZE 20//(8 * 1024 * 1024)

/* EMC clock delay */
#define CLK0_DELAY 7

void Chip_SystemInit(void)
{
/* Initial internal clocking */
//Chip_SetupIrcClocking();

/* Setup FLASH acceleration to target clock rate prior to clock switch */
Chip_CREG_SetFlashAcceleration(MAX_CLOCK_FREQ);

Chip_SetupXtalClocking();

/* Reset and enable 32Khz oscillator */
LPC_CREG->CREG0 &= ~((1 << 3) | (1 << 2));
LPC_CREG->CREG0 |= (1 << 1) | (1 << 0);
}

void EMC_SetpinMux

{


/* EMC Address Lines */
/*A0 - A4*/
Chip_SCU_PinMuxSet(0x02, 9, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
Chip_SCU_PinMuxSet(0x02, 10, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
Chip_SCU_PinMuxSet(0x02, 11, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
Chip_SCU_PinMuxSet(0x02, 12, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
Chip_SCU_PinMuxSet(0x02, 13, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));

/*A5 - A7*/
Chip_SCU_PinMuxSet(0x01, 0, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));
Chip_SCU_PinMuxSet(0x01, 1, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));
Chip_SCU_PinMuxSet(0x01, 2, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));

/*A8 - A10*/
Chip_SCU_PinMuxSet(0x02, 8, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
Chip_SCU_PinMuxSet(0x02, 7, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
Chip_SCU_PinMuxSet(0x02, 6, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));

/*A11 - A13*/
Chip_SCU_PinMuxSet(0x02, 2, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));
Chip_SCU_PinMuxSet(0x02, 1, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));
Chip_SCU_PinMuxSet(0x02, 0, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));

/*A14-A15*/
Chip_SCU_PinMuxSet(0x06, 8, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC1));
Chip_SCU_PinMuxSet(0x06, 7, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC1));


/* EMC Data Lines */
/* D0 - D7 */
Chip_SCU_PinMuxSet(0x01, 6, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
Chip_SCU_PinMuxSet(0x01, 7, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
Chip_SCU_PinMuxSet(0x01, 8, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
Chip_SCU_PinMuxSet(0x01, 9, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
Chip_SCU_PinMuxSet(0x01, 10, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
Chip_SCU_PinMuxSet(0x01, 11, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
Chip_SCU_PinMuxSet(0x01, 12, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
Chip_SCU_PinMuxSet(0x01, 13, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));

/* D8 - D11 */
Chip_SCU_PinMuxSet(0x05, 4, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));
Chip_SCU_PinMuxSet(0x05, 5, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));
Chip_SCU_PinMuxSet(0x05, 6, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));
Chip_SCU_PinMuxSet(0x05, 7, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));

/* D12 - D15 */
Chip_SCU_PinMuxSet(0x05, 0, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));
Chip_SCU_PinMuxSet(0x05, 1, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));
Chip_SCU_PinMuxSet(0x05, 2, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));
Chip_SCU_PinMuxSet(0x05, 3, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC2));


/*EMC Control Lines*/
/*EMC_WE*/
Chip_SCU_PinMuxSet(0x01, 6, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));

/*EMC_BLS0*/
Chip_SCU_PinMuxSet(0x01, 4, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));
/*EMC_BLS0*/
Chip_SCU_PinMuxSet(0x06, 6, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC1));

/*EMC_CAS*/
Chip_SCU_PinMuxSet(0x06, 4, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));

/*EMC_RAS*/
Chip_SCU_PinMuxSet(0x06, 5, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));

/*SDRAM_CS0*/
Chip_SCU_PinMuxSet(0x06, 9, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));

/*SDRAM_CKEO (EMC_CKEOUT0)*/
Chip_SCU_PinMuxSet(0x06, 11, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));

/*EMC_DQMOUT0*/
Chip_SCU_PinMuxSet(0x06, 12, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));

/*EMC_DQMOUT1*/
Chip_SCU_PinMuxSet(0x06, 10, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC3));

/* SDRAM_CLK0 (EMC_CLK0)*/
Chip_SCU_ClockPinMuxSet(0, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_HIGHSPEEDSLEW_EN | SCU_MODE_FUNC0));

}

void EMC_SetupSDRAMMemmory(void)
{

/* Setup EMC Delays */
/* Move all clock delays together */
LPC_SCU->EMCDELAYCLK = ((CLK0_DELAY) | (CLK0_DELAY << 4) | (CLK0_DELAY << 8) | (CLK0_DELAY << 12));

/* Setup EMC Clock Divider for divide by 2 - this is done in both the CCU (clocking)
and CREG. For frequencies over 120MHz, a divider of 2 must be used. For frequencies
less than 120MHz, a divider of 1 or 2 is ok. */
Chip_Clock_EnableOpts(CLK_MX_EMC_DIV, true, true, 2);
LPC_CREG->CREG6 |= (1 << 16);

/* Enable EMC clock */
Chip_Clock_Enable(CLK_MX_EMC);

/* Init EMC Controller -Enable-LE mode */
Chip_EMC_Init(1, 0, 0);
/* Init EMC Dynamic Controller */
Chip_EMC_Dynamic_Init((IP_EMC_DYN_CONFIG_T *) &AS4C4M16SA_CI_Config);

}

/*Main While*/

uint32_t *StardAddr, *StardAddr1;
uint32_t Length = DRAM_SIZE;
uint32_t ReadData[DRAM_SIZE];
uint32_t WriteData[DRAM_SIZE];
unsigned long i = 0;

int main(void)
{

#if defined (__USE_LPCOPEN)
// Read clock settings and update SystemCoreClock variable
SystemCoreClockUpdate();

#endif

// TODO: insert code here
/* LED31 PA.4 - GPIO5[19] */
Chip_SCU_PinMuxSet(0xA, 4,(SCU_MODE_INBUFF_EN | SCU_MODE_PULLUP | SCU_MODE_FUNC4));
Chip_GPIO_SetPinState(LPC_GPIO_PORT, 5, 19, (bool) true);
Chip_GPIO_SetPinDIROutput(LPC_GPIO_PORT, 5, 19);

EMC_SetPinMux();
// Force the counter to be placed into memory
EMC_SetupSDRAMMemmory();
// Enter an infinite loop, just incrementing a counter


while(1)
{
StardAddr = (uint32_t *)EMC_ADDRESS_DYCS0;
for(i=0; i<20; i++)
{
*StardAddr = 0x55AA55AA;
StardAddr++;
}
for (i=0; i<0xFFFF;i++ );
for (i=0; i<0xFFF;i++ );
#if 1
StardAddr1 = (uint32_t *)EMC_ADDRESS_DYCS0;
for(i=0; i<Length; i++)
{
ReadData[i] = (uint32_t)*StardAddr1;
if(ReadData[i] != *StardAddr1)
{
while(1)
{
Chip_GPIO_SetPinToggle(LPC_GPIO_PORT, 5, 19);
for (i=0; i<0xFFFFF;i++ );
}
}
StardAddr1++;
}
#endif


}
return 0 ;
}

I am not understanding that it sometimes works and sometime while debugging it crasches. I referred  follwing thread

https://community.nxp.com/thread/455171 while implementation. 

Please let me now whether the method whic i am using to access the SDRAM memory is correct?

Also find the code attached for reference.

Thanks 

Gaurav More

0 项奖励
回复

1,314 次查看
gauravmore
Contributor III

Hi Jeremy,

Please refer the issue link mentioned .

https://community.nxp.com/t5/LPC-Microcontrollers/Issue-in-Allocation-of-Variable-in-External-RAM-SD...

 

Kindly reply for the same.

BR,

Gaurav More

 

 

0 项奖励
回复

1,346 次查看
gauravmore
Contributor III

Hi Jeremy,

Any inputs regarding the query. It is required for  the project development. Need to any modifications required since some times it runs a complete while and agian while repeating the same statement it crashes,

while(1)
{
StardAddr = (uint32_t *)EMC_ADDRESS_DYCS0;
for(i=0; i<20; i++)
{
*StardAddr = 0x55AA55AA;
StardAddr++;
}
for (i=0; i<0xFFFF;i++ );
for (i=0; i<0xFFF;i++ );
#if 1
StardAddr1 = (uint32_t *)EMC_ADDRESS_DYCS0;
for(i=0; i<Length; i++)
{
ReadData[i] = (uint32_t)*StardAddr1;
if(ReadData[i] != *StardAddr1)
{
while(1)
{
Chip_GPIO_SetPinToggle(LPC_GPIO_PORT, 5, 19);
for (i=0; i<0xFFFFF;i++ );
}
}
StardAddr1++;
}
#endif

refer the code attached inthe above post.

Thanks 

Gaurav More

0 项奖励
回复