SDR on LPC4357

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDR on LPC4357

1,775 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blu on Thu Feb 04 15:53:08 MST 2016
Hello I am planning to use 8 MB SDRAM on on LPC4357 for grx applications. I would need something that works seamlessly with EMC on LPC4357. The LPC4357 EVB uses 32 MB from Micron but winbond offers the same size for much cheaper price. Please suggest if LPC4357 EMC is compatible with winbond's SDR ?
标签 (1)
0 项奖励
回复
2 回复数

1,731 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blu on Tue Feb 23 20:24:47 MST 2016
Hi MC,

Can you suggest which spec I need to check on LPC4357 to ensure the timings would match with the below SDRAM?
https://www.winbond.com/resource-files/w9825g2jb_a01.pdf

It can go up to 166MHz
0 项奖励
回复

1,731 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Thu Feb 04 21:39:25 MST 2016
Hi blu,
LPC4357 should be able to support most of the SDRAMs. You need to check SDRAM timing and compare with LPC4357 timings. Which SDRAM are you planning to use?
0 项奖励
回复