SDR SDRAM PROBLEM(RESET PROBLEM) IN LPC3250

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDR SDRAM PROBLEM(RESET PROBLEM) IN LPC3250

975件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MOHAMMAD BIYABANI on Tue Feb 12 00:19:34 MST 2013
Hi,now i am working with LPC3250 controller with two SDR SDRAM(MT48LC32M16A2)  were interfaced.Already i worked with one  SDRAM at that time information is loaded successfully(kernel booted successfully).But now i am getting problem with two SDRAM'SThe problem is after kernel booted board reset automatically? how to rectify it? . I have another  doubt if we use another sdram (in past i used 32Mb SDR SDRAM now i am using 512Mb((MT48LC32M16A2)) then can we have to change the timing parameters or not?If we have to change then what are the parameter values?please reply..
thanks in advance...
ラベル(1)
0 件の賞賛
返信
0 返答(返信)