SDMMC driver with Interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDMMC driver with Interrupt

1,552 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by viswanath on Sat Apr 13 13:33:31 MST 2013

Hi,


Need help in the Interrupt implementation for SDMMC driver.


I enabled the interrupt in the control register in the function: sdio_init as:LPC_SDMMC->CTRL = MCI_CTRL_USE_INT_DMAC | MCI_CTRL_INT_ENABLE;


anf i enabled the LPC_SDMMC->RINTSTS = 0xFFFFFFCE;(which implies Rx,TX Interrupt and CDET(card detect)). and i masked the below register.               (// LPC_SDMMC->TMOUT = 0xFFFFFFFF;).


but i didnt got any Interrupt. in SDIO_IRQHandler. i added few the status checking for the above 3 functionalities.


I am having small doudt like MCI_CTRL_USE_INT_DMAC  is the internal DMA so need to enable in the internal DMA registers.


Please suggest the right way.


Thanks & Regards,


Viswanath K.


 


 


标签 (1)
0 项奖励
回复
0 回复数