SDMMC driver with Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDMMC driver with Interrupt

1,515件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by viswanath on Sat Apr 13 13:33:31 MST 2013

Hi,


Need help in the Interrupt implementation for SDMMC driver.


I enabled the interrupt in the control register in the function: sdio_init as:LPC_SDMMC->CTRL = MCI_CTRL_USE_INT_DMAC | MCI_CTRL_INT_ENABLE;


anf i enabled the LPC_SDMMC->RINTSTS = 0xFFFFFFCE;(which implies Rx,TX Interrupt and CDET(card detect)). and i masked the below register.               (// LPC_SDMMC->TMOUT = 0xFFFFFFFF;).


but i didnt got any Interrupt. in SDIO_IRQHandler. i added few the status checking for the above 3 functionalities.


I am having small doudt like MCI_CTRL_USE_INT_DMAC  is the internal DMA so need to enable in the internal DMA registers.


Please suggest the right way.


Thanks & Regards,


Viswanath K.


 


 


ラベル(1)
0 件の賞賛
返信
0 返答(返信)